1670CT0701

Main Circuit Breakers

HDL

  • 125 A maximum field-installable EDB, EGB, or EJB
    (100 A max at 600Y/347 Vac)

  • 125 A maximum field-installable HD, HG, HJ, HL, or HR

  • 250 A maximum field-installable JD, JG, JJ, JL, or JR

  • 400 A maximum field-installable LA, LH ,LG, LJ, LL, or LR*

  • 600 A maximum field-installable LG, LJ, LL, or LR*

  • 800 A maximum factory installed MG, PG, PJ, or PL

Circuit Breaker Kits and Accessories

LAL Circuit Breaker

PowerPacT™ H-, J-, and L-frame circuit breakers are available with shunt trip, ground fault shunt trip, undervoltage trip, time delay, auxiliary switches, and alarm switches.

Field-installable undervoltage release, alarm switch, shunt trip, and auxiliary contacts are available for LA, and LH main circuit breaker interiors.

NOTE: See Supplemental Digest for additional accessories.

Main Circuit Breaker Adapter Kits (Circuit Breaker Not Included)

Adapter Kit Catalog Number Ampere Rating Main Circuit Breaker*

N150MH*

15–125 A* HD, HG, HJ, HL, HR

N250MJ

150–250 A JD, JG, JJ, JL, JR

N400M

125–400 A LA, LH

N600MPPL*

400–600 A LG, LJ, LL or LR
N250MJ Main Circuit
Breaker Kit
N400M Main Circuit
Breaker Kit
N600MPPL Main Circuit
Breaker Kit
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.