1670CT0701

Power and Energy Management Options

Several Power Meters and Circuit Monitors are available factory-assembled in most NF panelboards. Basic Energy Metering at the Mains is possible with PowerLogic™ EM3500 series circuit monitors. Power Quality Monitoring is available with the selection of PM5563 or PM8244 power meters. These are typically installed with an LCD display in a 7 inch (178 mm) wide side gutter. Communications from these meters is avaiable via Ethernet Modbus TCP/IP.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.