1670CT0701

Typical Wiring Diagrams

1-Phase, 3-Wire  
125–250 A Main Lugs   125 A Max. Branch Mounted Main Circuit Breaker   15–250 A Main Circuit Breaker Types H-, or J-Frame  
400–600 A Main Lugs   400 A Max. Main Circuit Breaker Type LA/ LH Frame      
400 A or 600 A PowerPacT L-Frame Main Circuit Breaker with Feed-Thru Lugs   400 A or 600 A PowerPacT L-Frame Main Circuit Breaker with Sub-feed Circuit Breaker      
NF 800 A Main Lugs NF 800 A Max. Main Circuit Breaker—(M- or P-Frame)  
3-Phase, 4-Wire
125–250 A Main Lugs 125 A Max. Branch Mounted Main Circuit Breaker 15–250 A Main Circuit Breaker Types H-, or J-Frame
     
400–600 A Main Lugs 400 A Max. Main Circuit Breaker Type LA/LH Frame  
400 A or 600 A PowerPacT
L-Frame Main Circuit Breaker with Feed-Thru Lugs
400 A or 600 A PowerPacT
L-Frame Main Circuit Breaker with Sub-feed Circuit Breaker
 
     
NF 800 A MLO—3PH, 4W 800 A Max. Main Circuit Breaker (M- or P-Frame)  
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.