Assign Model Names and Autoupdaters

Assign the following model names and autoupdaters using the ArcFM Properties Manager. 

Conduit feature class

Model Name: ULS

Field Model Names:

Field

Field Model Name

DuctBankConfiguration

DUCTBANKCONFIGURATION

DuctBankHeight

DUCTBANKHEIGHT

DuctBankWidth

DUCTBANKWIDTH

Special Autoupdaters:

Event

Autoupdater

On Feature Update

ArcFM Check Cross Section

Cable (e.g. Conductor or Fiber Cable) Feature Classes

Model Name: ULSMEMBER

Special Autoupdaters:

Event

Autoupdater

On Feature Update

ArcFM Check Cross Section

On Feature Delete

ArcFM Remove Deleted ULS Member

Field Model Name: CABLECOUNT

TIP: The CABLECOUNT field model name is optional and used to support the Cable Count field. This model name runs a validation that ensures the Cable Count set at the feature class level matches the Cable Count chosen in the ArcFM Conduit Association Editor. See the Using Guide topic Number of Cables for more information.
  • With the field model name assigned, the application ensure the counts match.

  • Without the field model name assigned, no validation is performed. This means the Cable Count fields might differ. If your company does not leverage the concept of Cable Count, you could remove this attribute field entirely, if desired.

Cross Section Annotation feature class

Model Name: CROSSSECTION

IMPORTANT: This model name can only be assigned to one annotation feature class.

Duct Definition object class

Model Name: DUCT

Field Model Names:

Field

Field Model Name

ActualSize

ACTUALDUCTSIZE

Availability

DUCTAVAILABILITY

BypassIDFrom

BYPASSIDFROM

BypassIDTo

BYPASSIDTO

ContinuingDuctNameFrom

CONTINUINGDUCTNAMEFROM

ContinuingDuctNameTo

CONTINUINGDUCTNAMETO

DuctID

DUCTID

DuctSize

DUCTSIZE

Material

DUCTMATERIAL

Conduit_Cable Relationship Class

Relationship Autoupdaters:

IMPORTANT: If you plan to also implement Underground Facility Manager, assign the ArcFM Conduit to Conductor Composite autoupdater. This AU calls both the ArcFM Manage Conduit Manager Relationship Changes AU and the ArcFM UFM Conduit to Conductor Relationship AU.

Event

Autoupdater

On Relationship Created

ArcFM Manage Conduit Manager Relationship Changes OR ArcFM Conduit to Conductor Composite, depending on whether you plan to implement UFM.

On Relationship Updated

ArcFM Manage Conduit Manager Relationship Changes OR ArcFM Conduit to Conductor Composite, depending on whether you plan to implement UFM.

On Relationship Deleted

ArcFM Manage Conduit Manager Relationship Changes OR ArcFM Conduit to Conductor Composite, depending on whether you plan to implement UFM.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.