Add Model Names

Add model names to domains by right-clicking the geodatabase and selecting Properties. Note that some of the model names listed below may exist in other domains (e.g., SYMBOLROTATION, INSETFRAMESOURCE may exist in Domain Independent Field Model Names domain). You may assign these model names from a different domain or add them to the electric domains mentioned below. The various domains are primarily to help you organize your model names logically.

TIP:
  • If it has been a while since you’ve added model names, helpful steps are included in the Conduit Manager Add Model Names topic.

  • While you are verifying or adding the model names below, you can tackle the Conduit Manager Add Model Names at the same time!


Class Model Names

Add the following model names to the Electric Object Class Model Name domain. Some may already exist. They must have the exact spelling as shown.

MANHOLEFEATURESNAP

STRUCTURE

UFMANCHOR

UFMANNOTATION

UFMDIMENSION

UFMDUCT

UFMDUCTBANK

Field Model Names

Add the following field model names to the Electric Field Model Name domain. Some may already exist. They must have the exact spelling as shown.

BYPASSID

CONTINUINGDUCTNAME

DUCTAVAILABILITY

DUCTID

DUCTMATERIAL

DUCTNAME

DUCTOCCUPIED

DUCTOCCUPANCY

DUCTSIZE

DUCTTYPE

DUCTUNAVAILABLEREASON

FACILITYDIAGRAM

FACILITYID

HASSUBDUCTS

PHASEDESIGNATION

WALLGRIDORIGIN

WALLGRIDCELLSIZE

SYMBOLROTATION (should be in the Domain Independent Field Model Name domain)

INSETFRAMETITLE (should be in the Domain Independent Field Model Name domain)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.