Conduit Trace Criteria Configuration

The Conduit Trace Criteria tool requires some database configuration for the enhanced functionality to work properly. Follow the steps below to complete the required configuration.

  1. Add the following Coded Values to the Electric Field Model Names:

    Code

    Description

    DUCTTYPE

    DUCTTYPE

    DUCTUNAVAILABLEREASON

    DUCTUNAVAILABLEREASON

  2. Add a new Domains for Duct Type and Duct Unavailability Type including their Coded Values as outlined below:

    Duct Type

    Domain Property

    Value

    Domain Name

    Duct Type

    Field Type

    Text

    Domain Type

    Coded Values

    Split Policy

    Default Value

    Merge policy

    Default Value

    Code

    Description

    Electric Distribution

    Electric Distribution

    Electric Transmission

    Electric Transmission

    Communication

    Communication

    Duct Unavailability Type

    Domain Property

    Value

    Domain Name

    Duct Unavailability Type

    Field Type

    Text

    Domain Type

    Coded Values

    Split Policy

    Default Value

    Merge policy

    Default Value

    Code

    Description

    None

    None

    Full

    Full

    Obstructed

    Obstructed

  3. Add two new fields to the Duct Definition table and assign domains to each as indicated below:

    1. Field Name: DuctType

      Data Type: Text

      Field Properties

      Value

      Alias

      DuctType

      Allow NULL Values

      Yes

      Domain Value

      (This can be left empty.)

      Domain Type

      Duct Type

      Length

      25

    2. Field Name: UnavailabilityReason

      Data Type: Text

      Field Properties

      Value

      Alias

      UnavailabilityReason

      Allow NULL Values

      Yes

      Domain Value

      (This can be left empty.)

      Domain Type

      Duct Unavailability Type

      Length

      25

  4. Assign a Field Model Name to the DuctType field for DUCTDEFINITION.

    1. For Model Name Domain, select Electric Field Model Names from the drop-down.

    2. Then add DUCTTYPE to the Selected column.

  5. Assign a Field Model Name to the UnavailabilityReason field for DUCTDEFINITION.

    1. For Model Name Domain, select Electric Field Model Names from the drop-down.

    2. Then add DUCTTYPE to the Selected column.

  6. Add two new Fields and apply Domains as follows to the Duct feature class:

    Field Name: DuctType

    Data Type: Text

    Field Properties

    Value

    Alias

    DuctType

    Allow NULL Values

    Yes

    Domain Value

    (This can be left empty.)

    Domain Type

    Duct Type

    Length

    50

    Field Name: DuctUnavailabilityReason

    Data Type: Text

    Field Properties

    Value

    Alias

    Duct Unavailability Reason

    Allow NULL Values

    Yes

    Domain Value

    (This can be left empty.)

    Domain Type

    Duct Unavailability Type

    Length

    50

  7. Assign a Field Model Name to the DuctType field for Duct.

    1. For Model Name Domain, select Electric Field Model Names from the drop-down.

    2. Then add DUCTTYPE to the Selected column.

  8. Assign a Field Model Name to the DuctUnavailabilityReason field for Duct.

    1. For Model Name Domain, select Electric Field Model Names from the drop-down.

    2. Then add DUCTTYPE to the Selected column.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.