Using Feeder Sync with Geodatabase Manager (GDBM)

  1. Configure the Feeder Sync Tool via the Feeder Manager Configuration window.
  2. Add the following Action Handlers for the Feeder Sync Tool to your existing GDBM configuration (see the Tasks topic for more information):
    • Run Feeder Sync assigned to Before Post.

    • Cleanup Feeder Sync assigned to After Post.

  3. Once GDBM has been properly configured for the Feeder Sync Tool, open ArcMap and create a new Session or Design.
  4. Perform typical editing operations (create/delete features, editing existing features, etc.) in that session or design.
    • Notice that the Feeder Information fields from Feeder Manager 2.0 update after each edit (Feeder IDs, Subfeeder IDs (if applicable), Energized Phases, Number of Feeders, Loop, Tie Device).

    • Notice that the Feeder Information in the legacy fields (FeederID, FeederID2 and FeederInfo) does not update after each edit.

  5. Save the session or design. This populates the MM_EDITED_FEATURES table. You can add the MM_EDITED_FEATURES table to inspect its contents if necessary.
  6. Send the Session or Design to the GDBM Post Queue.
  7. After GDBM runs through the posting process you can inspect the Logging tab for information on the number of features synced and if it was completed successfully.

  8. Open your SDE. Default version in ArcMap and inspect the legacy FeederID, FeederID2, and FeederInfo fields to see that they have been updated.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.