CompleteAssignmentTrigger

Node Action:

This node action is used in the entry node of a workflow to specify that when a single session is selected in the Session Manager window, a button appears in the list of buttons under the Workflows section that triggers the workflow when clicked.

Parameters:

se_type

CompleteAssignmentTrigger

se_type = CompleteAssignmentTrigger

se_visibilityCondition

se_visibilityCondition = "(ctx, log) => { return false; }"

Contains code that must return a bool indicating when the workflow button should be visible in the respective list of buttons in Session Manager.

se_displayName

The display name of the workflow button in Session Manager.

se_iconUrl

The URL for the icon of the workflow button in Session Manager.

se_iconService

The service for the icon of the workflow button in Session Manager.

se_iconXaml

se_iconXaml = "
    <Canvas
        Width=\"20\"
        Height=\"20\"
        Margin=\"1\"
        SnapsToDevicePixels=\"True\">

        <!-- Insert Icon Components -->

    </Canvas>
"

The XAML for the icon of the workflow button in Session Manager.

se_sortOrder

The order in which the workflow button appears in the list of buttons in Session Manager.

Example

Complete Assignment with Icon Url: This example illustrates how to properly use the CompleteAssignmentTrigger node action, where the icon is defined by a URL.

digraph workflow {

  entry[
    se_type0 = CompleteAssignmentTrigger,
    se_displayName0 = "Complete Assignment"
    se_iconUrl0 = "https://mysubscription.blob.core.windows.net/img/assignmentIcon.png"
    se_requiresConnection0 = false,
    se_sortOrder0 = 100,
    se_visibilityCondition0 = "(ctx, log) => {
      return ctx.Event.assignment.assignedTo == ctx.User.UserId && ctx.Event.isSessionOpen == true;
    }"
  ]
  
  exit[
    shape = invhouse, 
    color = "#22FF44", 
    style = filled
  ]
  
  entry -> exit
}
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.