RequestDesignSave
Node Action:
The RequestDesignSave node action causes Designer XI to save the design.
Parameters:
se_type
RequestDesignSave
se_type = RequestDesignSavese_promptUserIfDirty
Shows the "Would you like to save" prompt if there are changes.
se_resultVariable
A variable to set if the design was saved.
Example:
Update Property And Save: Updates a property on a component and saves the design.
digraph workflow {
entry[
se_type0 = ComponentToolTrigger,
se_displayName0 = "Update And Save"
se_iconService0 = ""
se_iconUrl0 = ""
se_requiresConnection0 = false,
se_sortOrder0 = 0,
se_visibilityCondition0 = "(dynamicStateMachineContext, msLogger) => {
return true;
}",
]
UpdateAndSave[
se_type0 = SetPropertyOnComponent,
se_determineComponentId0 = "(dynamicStateMachineContext, msLogger) => {
return dynamicStateMachineContext.Event.component.id.ToString();
}",
se_propertyName0 = "NewProperty"
se_value0 = "NewValue"
se_type1 = RequestDesignSave,
se_promptUserIfDirty1 = false,
se_resultVariable1 = Saved
]
entry->UpdateAndSave->exit
}