PrintToolTrigger

Node Action:

This is a workflow trigger that places a button under the print tool drop-down.

Parameters:

se_type

PrintToolTrigger

se_type = PrintToolTrigger

se_displayName

The display name of the workflow button under the print tool.

se_iconUrl

The URL for the icon of the workflow button under the print tool.

se_iconService

The service for the icon of the workflow button under the print tool.

se_requiresConnection

A bool to require internet connectivity.

se_sortOrder

The order in which the workflow button appears under the print tool.

Example

Print Tool Trigger: This example illustrates how to properly use the PrintToolTrigger node action.

digraph workflow {

  entry[
    se_type0 = PrintToolTrigger,
    se_displayName0 = "Attach Construction Print"
    se_iconService0 = ""
    se_iconUrl0 = ""
    se_requiresConnection0 = false,
    se_sortOrder0 = 200,
  ]
  
  exit[
    shape = invhouse, 
    color = "#22FF44", 
    style = filled
  ]
  
  entry -> exit
}
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.