DesignSavedTrigger

Node Action:

This is a workflow trigger that fires when the design is saved.

Parameters:

se_type

DesignSavedTrigger

se_type = DesignSavedTrigger

se_triggerCondition

Contains code that must return a bool indicating when the trigger should fire.

se_requiresConnection

A bool to require internet connectivity to run.

Example

Design Saved Trigger: This example illustrates how to properly use the DesignSavedTrigger node action.

digraph workflow {

  entry[
    se_type0 = DesignSavedTrigger,
    se_requiresConnection0 = false,
    se_triggerCondition0 = "(dynamicStateMachineContext, msLogger) => {
      return dynamicStateMachineContext.Event.assignment.status.ToString() == \"InProgress\";
    }"
  ]
  
  exit[
    shape = invhouse, 
    color = "#22FF44", 
    style = filled
  ]
  
  entry -> exit
}
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.