Triggers

Triggers are a subset of node actions that, when used on the entry node of a workflow, tell certain aspects of an XI series application where and how that workflow can be triggered. Each topic in this section provides triggers, their parameters, and examples.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.