DeepLinkTrigger

Node Action:

This is a workflow trigger that fires when an arcfmdxi deeplink with a handlerName DeepLinkTriggerAction is clicked. The WorkflowAncestralId parameter determines which workflow should be triggered..

Parameters:

se_type

DeepLinkTrigger

se_type = DeepLinkTrigger

Example

Deep Link Trigger: This example illustrates how to properly use the DeepLinkTrigger node action. An example deeplink looks like `arcfmdxi://?handlerName=DynamicWorkflowManager&WorkflowAncestralId=29b3603e-de6a-4ff1-8fad-3417a4f75b4d&arg1=value1&arg2=value2`.

digraph workflow {

  entry[
    se_type0 = DeepLinkTrigger,
      ]
  
  exit[
    shape = invhouse, 
    color = "#22FF44", 
    style = filled
  ]
  
  entry -> exit
}
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.