Node Actions

Node actions are the crucial building blocks in dynamic workflows that enable the use of vital pieces of functionality, such as issuing REST API calls and zooming to a component. Each topic in this section provides node actions, their parameters, and examples.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.