RefreshWorkList

Node Action:

The RefreshWorkList node action refreshes the assignments, work requests, and design resources. It will also refresh the custom properties for the backstage.

Parameters:

se_type

RefreshWorkList

se_type = RefreshWorkList

Example:

Refresh Work List: A button to refresh the backstage..

digraph workflow {

entry[
se_type0 = BackstageToolTrigger,
se_displayName0 = "Refresh All"
se_iconService0 = ""
se_iconUrl0 = ""
se_requiresConnection0 = false,
se_sortOrder0 = 0,
se_visibilityCondition0 = "(dynamicStateMachineContext, msLogger) => {
  return true;
}",

se_type1 = RefreshWorkList,

]
entry->exit
}
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.