NotifyUser

Node Action:

The NotifyUser node action sends a notification to the user. This can be shown as a toast message.

Parameters:

se_type

NotifyUser

se_type = NotifyUser

se_message

The notification message.

se_showToast

Whether to show the message in a toast too.

se_determineMessage

A lambda to build a message.

se_notificationType

The notification types can be Alert, Information, or Completed.

Example:

Get DSR Representation: Copies the Design State Resource (DSR) to the clipboard and notifies the user when completed.

digraph finite_state_machine { 

  splines=spline; 
  edge[arrowsize=1, color=black];
  node[shape = box, color = green];
  
  entry[
    label = "Copy Design Inf to Clipboard",
    shape= invhouse,
    height = 1,
    
    se_type2 = DesignToolTrigger,
    se_displayName2 = "Copy Design Info (DT)"
    se_iconUrl2 = "https://arcfmazuredev.blob.core.windows.net/img/CompleteDesign.png",   
    se_deferUntilOnline2 = false,
    se_requiresInternet2 = true,
    se_sortOrder2 = 0,
    se_visibilityCondition2 = "function (ctx, msLogger) {
      return true && ctx.Event.design.name != \"Demo - 2024.03.15.01\";
    }"    
    
    se_type6 = GetDesignStateResource,
    se_determineAssignmentId6 = "function (ctx, msLogger) {
      return ctx.Event.assignment.id;
    }",
    se_resultVariable6 = Dsr
  ]; 
  
  exit[
    label= "Complete", 
    shape=invhouse, 
    color="#22FF44", 
    style=filled,
    
    se_type1 = Action,
    se_action1 = "function (ctx, log) {
      ctx.Output.Cancel = true;
    }",
  ];
  
  copyToClipboard[
    label = "Copy to Clipboard"
    se_type1 = CopyToClipboard,
    se_determineData1 = "function (ctx, log) {
      var newtonsoft = importNamespace('Newtonsoft.Json');
      return newtonsoft.JsonConvert.SerializeObject(ctx.State.Dsr);
    }",
  ]
  
  showToast[
    label = "Notify User Copy Succeeded",
    se_type1 = NotifyUser,
    se_message1 = "Component Details Copied to Clipboard",
  ]
  
  entry->copyToClipboard;
  copyToClipboard->showToast;
  showToast->exit;
  
  
}
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.