Asset Details Layout

The Asset Categories Layout tab lets you add widgets to the layout of the asset category to see specific data at a quick glance. Most of the widgets pull in the relevant data and add the tile to the layout window.

These widgets must be configured before they are added:

  • Asset metrics — create the metric label and then add metric fields to create the layout block.

  • Asset time series — show data points over a time range.

  • Asset Duval triangle and pentagon — see dissolved gas information in a color-coded pentagon or triangle.

  • Asset gauge — combine asset data values in to a gauge.

  • Asset time series histogram — see asset data values in a bar chart over time.

  • Asset table — create column names then add data fields to fill in the table.

After all the widgets are added, you can arrange the tiles on the page in any order. You can also import a layout from another workspace, and edit as needed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?