Asset Maintenance and Workflow
Calculation Workflow and Tasks
Automated tasks calculate information about asset categories. These tasks run calculations, such as elevation and location, that add factors to the asset data. Tasks can also run complex rule engines that help understand the life cycle of an asset based on the date it was installed, the predicted lifespan, and degradation over time.
Dismissed alarms
This tab shows all the alarms that were dismissed for this particular asset category. Use the text field search box to filter out different alarm names.
Maintenance Recommendations
A maintenance recommendation is an action used for an asset category to help scheduled tasks when specific alarms are triggered. These recommendations help you account for asset maintenance cost. This tab lets you configured different actions that are linked to both an alarm and intervention that were previously configured.
Advanced Properties Schema
The Advanced Properties Schema tab holds the asset properties configuration. Most categories have this information configured, but you can add new parameters to meet business needs. This is an example of one schema layout.