Facet Structure and Used Fields Columns

Facet structure is one of the global filters that you can use for narrowing down the list of assets in the main Asset Management System interface. As seen in the Global Filters topic, different filters show you groups of assets. Configuration of the facet structure is completed during implementation and can be seen in the workspace settings. Here is one example.


Fields in Tables

The list of assets in different tables and widgets can be configured in the Used fields tab. The window is broken up into different sections to set up.

  • filters

  • CNAIM asset drawer

  • vegetation asset drawer

  • charts widget

  • histogram widget

  • tables columns

  • tables widget columns

More rows can be added to each box. Here is an example.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?