Feeder Services Exports

Feeder Services exports are JSON files that represent a converted Esri UN model, enriched with catalog spec mappings, and compatible with your organization’s models (e.g., ADMS CIM model). Refer to the Create Geodatabase Regions (GRRs) and Mapping topics for information about creating GRRs and then grouping LV subnetworks together in the same GRR export.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?