Special Treatment of Closed Phases

To set the “ClosedPhases“ field correctly in the Geodatabase Region (GRR), you need to populate its value based on the “FeederServices/DisconnectedUnitSupport“ feature flag setting:

  • If the feature flag is set, the Phases property value is inserted into the “ClosedPhases“ property.

  • If the feature flag is not set, the Energized Phases property value is inserted into the “ClosedPhases“ property.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?