SurfacePolygonStructureResource
General purpose surface structure polygon component intended to be mapped to all surface structure polygon features.
|
Name |
Type |
Description |
|---|---|---|
|
componentType |
String |
"SurfacePolygonStructure" |
|
workflowState |
Int32 |
[Existing, AsBuilt, Proposed, Undefined, Modified] |
|
properties |
IDictionary |
Additional properties |
|
id |
Guid |
Unique identifier |
|
geometry |
IBoundedObject |
Geometric representation |
|
facilityId |
String |
Facility identifier |
|
esriId |
Int64 |
Esri identifier |
|
type |
String |
Type of structure |
|
isSubstation |
Boolean |
Indicates if it's a substation |
|
subnetworkName |
String |
Subnetwork name |
|
lifecycleStatusType |
LifecycleStatusType |
Lifecycle status |