View the Original Export Subnetwork JSON Data
There are times in which downstream systems from the GIS have existing integrations against Esri’s JSON. Feeder Services provides the identical benefits for GRR maintenance and integration with a new data format. Feeder Services also stores the original Export Subnetwork JSON data alongside the GRR data in the Storage Service.
To view the original Export Subnetwork JSON, perform the following steps:
- In Solution Center, click Feeder Services > Mapping > Geodatabase Regions.
- On the left side, click the desired GRR once to highlight
it in green.NOTE: You can use the Search field at the top of Solution Center to search for a GRR by its subnetwork name.
- At the end of the Esri Export JSON Storage ID field, click Download file to start a download of the underlying JSON file.
- Once the download is complete, click Show in folder to open File Explorer for the newly downloaded file.
- Open the file in a text editor, such as Notepad ++.