TrenchResource
Component used to represent Trench-type GIS features that do not have a geometry.
|
Name |
Type |
Description |
|---|---|---|
|
componentType |
String |
"Trench" |
|
id |
Guid |
Unique identifier |
|
esriId |
Int64 |
Esri identifier |
|
workflowState |
Int32 |
[Existing, AsBuilt, Proposed, Undefined, Modified] |
|
specId |
Guid |
Specification identifier |
|
properties |
IDictionary |
Additional properties |
|
facilityId |
String |
Facility identifier |
|
lifecycleStatusType |
LifecycleStatusType |
Lifecycle status |