NonSpatialFeederSourceResource
Resource used to represent a feeder source network component that does not have a spatial representation.
|
Name |
Type |
Description |
|---|---|---|
|
componentType |
String |
"NonSpatialFeederSource" |
|
workflowState |
Int32 |
[Existing, AsBuilt, Proposed, Undefined, Modified] |
|
properties |
IDictionary |
Additional properties |
|
id |
Guid |
Unique identifier |
|
operatingVoltage |
Voltage |
Operating voltage |
|
voltageClass |
Int32 |
[Primary, Secondary, Unknown] |
|
feederId |
String |
Feeder identifier |
|
distributionSystemType |
Int32 |
[Overhead, Underground, Submersible] |
|
facilityId |
String |
Facility identifier |
|
energizedPhases |
Int32 |
[None, C, B, BC, A, AC, AB, ABC, Unknown] |
|
closedPhases |
Int32 |
[None, C, B, BC, A, AC, AB, ABC, Unknown] |
|
sourceFeatureId |
Guid |
Source feature identifier |
|
energySource |
EnergySourceResource |
Energy source |
|
lifecycleStatusType |
LifecycleStatusType |
Lifecycle status |