Mapping

On the Mapping tab in the Feeder Services plugin are two sections, Maps and Geodatabase Regions (GRRs).

  • Maps – From the drop-down, select an operational map to act as your Network Feature Service. Feeder Services uses this map to create and update GRRs, and inform the application of your low voltage (LV) subnetworks to group within the GRR. Refer to the Choose an Operational Map topic for more information.

  • Geodatabase Regions – Click the Edit button to group LV subnetworks together in the same GRR export, rather than export them into separate GRRs. Refer to the Create Geodatabase Regions topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?