Sample Workflow in Action
Orchestration Trigger
The process for capturing and storing these states is automated in a number of OOTB Dynamic Workflows that are expected to run during normal business workflows. Descriptions of these can be found in the Dynamic Workflows topic. It is not expected that these workflows need to be customized, but an integration is needed to interface with Editor and Session Manager services to create a custom assignment with an AssignmentType of PatchValidation that triggers the ADMS Patch Integration orchestration.
Sample WMS Integration Workflow
One potential option for creating the custom assignment is through your Work Management System (WMS) that is integrated with a custom Dynamic Workflow. This is the recommended integration for customers using Designer XI as their design tool. These workflow step samples are also available in the Default Workflow Studio plugin within Solution Center.
-
After the design is approved through WMS, continue the workflow through Session Manager and Feeder Services before sending changes to ADMS.
-
Validate ADMS Patch Integration is enabled. This is optional but provides more QA/QC to prevent erroneously triggered workflows.
-
Get the Design and Work Request information from the Design Coordination Service.
-
Create the version and session in Session Manager XI and wait for a response.
Successful session creation:
-
Persist the version information to the Work Request resource.
-
Push To GIS makes the edits in the version associated with the session
-
Finally, once the edits have been applied, create the custom assignment in the Editor service.
Failed session creation:
In this path, an error message is generated to add to the Draw assignment, then reopens the assignment for a designer to view in Designer XI and resolve the issue(s).