DOCA0152EN-02

Firmware Version 004.000.009

New Features

  • Changed the maximum value of current in ERMS configuration to 15 x In.

  • When Instantaneous Current equals ERMS Current, ERMS mode is turned ON.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.