DOCA0152EN-02

Firmware Version 004.002.000

New Features

  • Improved the data availability, retry mechanism, and error handling in case of communication errors.

  • Improved the availability of BCM ULP module and synchronization in ULP network.

  • Improved the Modbus function code 100 – request handling.

Bugs Fixed

Communication between BCM ULP module and Modbus Interface (IFE or IFM interface) was lost, resulting in communication loss with Modbus master. The error was shown as slave address 99 or incorrect IP address.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.