DOCA0152EN-02

Firmware Version 004.001.005

New Features

In BCM ULP module with firmware version 004.001.004, added a reset feature for connecting to a MicroLogic type D trip unit.

Bugs Fixed

  • BCM ULP module with MicroLogic P or H trip units generated spurious alarms without tripping the BCM ULP system.

  • Ground-fault alarm and earth-leakage alarm were not displayed correctly for MicroLogic 6P, H, and MicroLogic 7P, H trip units.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.