DOCA0152EN-02

Firmware Version 004.001.007

New Features

  • Optimized the ULP bus load management for the ULP metering services when communicating with the IFE interface.

  • Resolved an internal reset issue that sometimes sent Breaker status not available to a supervisory system (for example, SCADA).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.