DOCA0152EN-02

Firmware Version 004.001.009

New Features

  • Improved the efficiency of handling multiple requests in BCM ULP module when requesting event log using FC20 or Protection command 63178.

  • Optimized the drift on reporting the trip cause and trip status.

  • Improved the functionality of Energy Reduction Maintenance Setting (ERMS) feature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.