DOCA0152EN-02

IO Module Synchronization after BCM ULP Firmware Update

WARNING
LOSS OF IO MODULE CONTROL FUNCTIONS
After updating the BCM ULP firmware, restart each IO module, either by pressing the IO Test/Reset button for 10–12 seconds or by switching Off/On the power to the IO module.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.