DOCA0152EN-02

BCM ULP Breaker Communication Module

Supplied with the circuit breaker, the BCM ULP module is installed behind the MicroLogic trip unit for MasterPact NT/NW, ComPact NS, and PowerPact P- and R-frame circuit breakers and is wired to the microswitches:

  • For manually operated devices:

    • OF, SDE, and SD contacts

  • For electrically operated devices:

    • OF, SDE, PF, and CH contacts

    • Connection kit to the MX1 and XF communicating voltage releases

The BCM ULP module is independent of the trip unit. It communicates two-way with:

  • ULP system via the circuit breaker ULP cord

  • MicroLogic trip unit via an infra-red link

  • Modbus network

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.