DOCA0152EN-02

Firmware Version 004.002.003

New Features

Optimized the log recording for MicroLogic Time Set events (Event 14/15).

Bugs Fixed

  • The BCM ULP module, which has recovered from Degraded mode was not listed in the IMU information webpage of IFE interface.

    NOTE: In the Degraded mode, there will be no communication with the trip unit for >60 s.
  • FC20 command was unable to read file30 records (event log of circuit breaker manager) when there was large number of records (≥8000 records).

  • Increments were inconsistent for the reset counter registers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.