DOCA0152EN-02

Firmware Version 004.001.004

New Features

  • BCM ULP module shares the earth-leakage alarm detector when connected to a MicroLogic 7.0 trip unit.

  • Improved the breaker status mask data based on the connected circuit breaker.

  • Improved the actuator mask data based on the connected circuit breaker.

Bugs Fixed

  • The MicroLogic alarm detectors were not shared when MicroLogic trip unit is not connected.

  • The ground-fault alarm was indicated when the connected MicroLogic trip unit does not support the feature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.