DOCA0140EN-03

Accessories

Accessories for ComPact NSX Circuit Breakers

A comprehensive accessory offer is available for ComPact NSX circuit breakers. Accessories can be installed on site to improve safety and ease of operation.

Sealed boot for the toggle handle, providing IP43 protection on the front

Short or long terminal shields, providing IP40 protection

Flexible interphase barriers improving isolation between power connections

For more information about the accessory offer, refer to LVPED217032EN,ComPact NSX & NSXm Catalogue.

Long Terminal Shields with Precut Grids

1 Cutting a grid

2 Adjusting the size of the grid

3 Inserting the grid in the terminal shield

Terminal shields with precut grids simplify the onsite connection of circuit breakers regardless of the number of conductors to be connected. The procedure for installing precut grids is described in the following instruction sheets on the Schneider Electric website:

  • GHD16242AA, ComPact NSX100–250 circuit breaker and switch-disconnector

  • GHD16243AA, ComPact NSX400–630 circuit breaker and switch-disconnector

Short Terminal Shields

The procedure for installing short terminal shields is described in the following instruction sheets on the Schneider Electric website:

  • GHD16242AA, ComPact NSX100–250 circuit breaker and switch-disconnector

  • GHD16243AA, ComPact NSX400–630 circuit breaker and switch-disconnector

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.