DOCA0140EN-03

Characteristics of MicroLogic Electronic Trip Units

Introduction

MicroLogic electronic trip units provide the following functions:

  • Protection of the electrical distribution or specific applications

  • Measurement of instantaneous values and measurement of average values (demand) for electrical quantities

  • Kilowatt hour metering

  • Operational assistance such as peak demand, customized alarms, and operation counters

  • Communication

Identification

Identify the trip unit installed on the circuit breaker by using the four characters on the front face:

 

Protection (X)

Case (Y)

Measurements (Z)

Application (T)

 

 

1
2
4
5
6
7


SI
LS0I
LS0IR
LSI
LSIG
LSIR

2

3

ComPact NSX100/160/250
ComPact NSX400/630


E

No measurement
Energy


G
AB
M
Z
AL

Distribution
Generator
Subscriber
Motor
16 Hz 2/3
Alarm

Examples

       

MicroLogic 1.3

SI

400 or 630 A

Distribution

MicroLogic 2.2 G

LS0I

100, 160 or 250 A

Generator

MicroLogic 2.3

LS0I

400 or 630 A

Distribution

MicroLogic 2.3 M

LS0I

400 or 630 A

Motor

MicroLogic 4.2

LS0IR

100, 160 or 250 A

Distribution including trip on earth leakage

MicroLogic 4.3 AL

LS0I

400 or 570 A

Distribution including alarm on earth leakage

MicroLogic 5.3 E

LSI

400 or 630 A

Energy

Distribution

MicroLogic 6.3 E-M

LSIG

400 or 630 A

Energy

Motor

MicroLogic 7.2 E-AL

LSI

100, 160 or 250 A

Energy

Distribution including alarm on earth leakage

MicroLogic 7.3 E

LSIR

400 or 630 A

Energy

Distribution including trip on earth leakage

Type of protection:
I Instantaneous
L Long-time
S0 Short-time (time delay cannot be adjusted)
S Short-time
G Ground-fault
R Residual (earth-leakage)

MicroLogic Trip Unit Families

The range of MicroLogic trip units is made up of several families:

  • MicroLogic 1, 2, and 4 without display screen

  • MicroLogic 5, 6, and 7 with display screen.

On MicroLogic 1, 2, and 4 trip units, the protection functions are set using adjustment dials on the front face of the trip unit:

On MicroLogic 5, 6, and 7 trip units, the protection functions are set:

  • By using the adjustment dials

  • By additional settings on the keypad. Setting values are displayed on the screen

  • Through EcoStruxure Power Commission software.

For more information about the MicroLogic 5, 6, and 7 trip units, refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide.

In Rating of MicroLogic Trip Units

The In rating (in amps) of a MicroLogic trip unit corresponds to the maximum value of the long-time protection (Ir) setting range for the trip unit. The setting range is indicated on the label on the front face of the trip unit (this label is visible on the front face of the ComPact NSX circuit breaker after the trip unit has been fitted).

Example: MicroLogic 5.2 E 250 trip unit:

  • Setting range: 100-250 A

  • In rating = 250 A

Distribution Trip Unit

The following figure and table define the protection functions for distribution-type MicroLogic trip units.

MicroLogic 5 and 6

MicroLogic 7

Item

Parameter

Description

MicroLogic(1)

2

4

5

6

7

A

Trip unit setting range: minimum setting/maximum setting.

The trip unit rating In corresponds to the maximum value of the Ir setting range.

 

O

O

O

O

O

B

Ir

Long-time protection pickup

L

C

tr

Long-time protection time delay

O

O

D

Isd

Short-time protection pickup

S

E

tsd

Short-time protection time delay

O

O

F

I2t ON/OFF

Short-time protection I2t curve in ON or OFF position

G

Ii

Instantaneous protection pickup

I

O

O

H

Ig

Ground-fault protection pickup

G

I

tg

Ground-fault protection time delay

J

I2t ON/OFF

Ground-fault protection I2t curve in ON or OFF position

K

IΔn

Earth-leakage protection pickup

R

L

Δt

Earth-leakage protection time delay

(1) Functions:
: Adjustable
O: Fixed
: Not present

Thermal Memory

The thermal memory is used to simulate temperature build-up and cooling in conductors caused by current variations, according to a time constant. In the event of an overload, the trip units with a thermal memory memorize the build-up temperature caused by the current. Memorizing the build-up temperature leads to a reduction in the trip time.

All MicroLogic trip units incorporate a thermal memory as standard:

  • For MicroLogic 2 and 4 trip units, the time constant is 15 minutes.

  • For MicroLogic 5, 6, and 7 trip units, the time constant is 20 minutes.

Motor Trip Units

The following figure and table define the protection functions for MicroLogic type M trip units.

Item

Parameter

Description

MicroLogic type M

1.3

2

6 E

A

Trip unit setting range: minimum setting/maximum setting.

The trip unit rating In corresponds to the maximum value of the setting range.

 

O

O

O

B

Ir

Long-time protection pickup

L

C

Class

Long-time protection trip class

D

Isd

Short-time protection pickup

S

E

tsd

Short-time protection time delay

O

O

O

F

Ii

Instantaneous protection pickup

I

O

O

O

G

Ig

Ground-fault protection pickup

G

H

tg

Ground-fault protection time delay

Iunbal

Phase-unbalance protection pickup

O

tunbal

Phase-unbalance protection time delay

O

(1) Functions:
: Adjustable
O: Fixed
: Not present

Motor Trip Unit: Additional Protection

MicroLogic type M trip units (in particular MicroLogic 6 E-M) also incorporate additional protection for the motor application. For more information, refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide..

Indication LEDs

Indication LEDs on the front of the trip unit indicate its operational state.

The LEDs and their meaning depend on the type of MicroLogic trip unit.

Type of MicroLogic trip unit

Description

Distribution

  • Ready LED (green): Blinks slowly when the electronic trip unit is ready to provide protection.

  • Overload pre-alarm LED (orange): Shows a steady light when the load exceeds 90% of the Ir setting.

  • Overload alarm LED (red): Shows a steady light when the load exceeds 105% of the Ir setting.

Motor

  • Ready LED (green): Blinks slowly when the electronic trip unit is ready to provide protection.

  • Overload temperature alarm LED (red): Shows a steady light when the motor thermal image exceeds 95% of the Ir setting.

The MicroLogic 1.3 M trip unit, which provides short-time protection only, displays the Ready LED (green).

The indication LEDs function for circuit breaker load currents:

  • Above 15 A on a MicroLogic trip unit rated 40 A

  • Above 30 A on MicroLogic trip units rated > 40 A

The limit value is indicated on the front panel, above the Ready LED of the MicroLogic trip unit.

NOTE: For the MicroLogic 4 and 7 trip units, the protection functions are supplied by a second power supply, in addition to the current transformer supply. The Ready LED blinks irrespective of the load, indicating that the standard protection functions are operational.

To activate the Ready LED when the load current is below the limit value, you can:

  • Install a 24 Vdc external power supply module which allows the trip unit to be monitored continuously, even when the circuit breaker is open. For more information, refer to LVPED217032EN, ComPact NSX & NSXm Catalogue.

  • Or, during maintenance visits, connect the pocket battery to monitor the trip unit.

NOTE: If the pre-alarm and alarm LEDs keep lighting up, perform load shedding to avoid tripping due to a circuit breaker overload.

Test Port

MicroLogic trip units feature a test port specifically for maintenance actions.

Use the test port to:

  • Connect a pocket battery for local testing of the MicroLogic trip unit

  • Connect the Service Interface for testing, setting the MicroLogic trip unit, updating the MicroLogic firmware, or for installation diagnostics with EcoStruxure Power Commission software

  • Connect the USB maintenance interface:

    • For push-to-trip test or installation diagnostics with the USB maintenance interface stand-alone

    • For testing and installation diagnostics, setting the MicroLogic trip unit, updating the MicroLogic firmware with the USB maintenance interface connected to a PC

NOTE: The test port is capped on the ComPact NSX400K circuit breaker.
WARNING
hazard of REDUCED INSULation distances
On a ComPact NSX400K circuit breaker, do not remove the cap on the MicroLogic test port.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Interchangeability of MicroLogic Trip Units

Onsite replacement of trip units is simple:

  • No connections to make

  • No specific tools (for example, calibrated torque wrench)

  • Compatibility of trip units provided by mechanical cap

  • Torque limited screw provides correct torque

The simplicity of the replacement process means that it is easy to make the necessary adjustments as operation and maintenance processes evolve.

NOTE: The screw head is accessible when the trip unit is installed, so the trip unit can still be removed.
NOTE: On ComPact NSX circuit breakers with NA, R, HB1, HB2, and K breaking performances the trip units are not interchangeable.

Sealing the Protection

Seal the transparent cover on MicroLogic trip units to prevent modification of the protection.

On MicroLogic 5, 6, and 7 trip units, it is possible to use the keypad, with the cover sealed, to read the protection settings and measurements.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.