DOCA0140EN-03

Environmental Conditions

Ambient Temperature

The ambient temperature refers to the temperature of the air immediately surrounding the circuit breaker.

  • Operation temperature

    • –25 to +70 °C (–13 to +158 °F): Normal operating temperature

      NOTE: The minimum operating temperature for the earth-leakage fault indicator on the MicroLogic 4 and 7 trip unit is -15 °C (5°F). Between -15 and -5 °C (5 and 23 °F), and when operating the device with an earth leakage fault and a very low load compared to the trip unit rating In, the earth leakage indicator may not work correctly (fault indication or reset).
    • –35 to –25 °C (–31 to –13 °F): Commissioning possible

  • Storage temperature

    • –50 to +85 °C (–58 to +185 °F): Without MicroLogic trip unit

    • –40 to +85 °C (–40 to +185 °F): With liquid crystal MicroLogic trip unit or PowerTag Energy

Extreme Atmospheric Conditions

ComPact NSX circuit breakers are designed to operate in industrial atmospheres as defined in standard IEC/EN 60947-2 for the highest level of pollution (level 3).

They are tested for extreme storage conditions according to the following standards:

Standard

Title

IEC/EN 60068-2-2

Dry heat, severity level +85 °C (+185 °F)

IEC/EN 60068-2-1

Dry cold, severity level –55 °C (–67 °F)

IEC/EN 60068-2-30

Damp heat, cyclic

  • temperature +55 °C (+131 °F)

  • relative humidity 95 %

IEC/EN 60068-2-52

Salt-mist test

To obtain the best use from the circuit breakers, install them in properly ventilated switchboards where excessive dust is not a problem.

Vibration

ComPact NSX circuit breakers are tested against vibration.

Conformity tests are carried out in accordance with standard IEC/EN 60068-2-6 at the levels of severity required by the merchant shipping regulatory bodies (IACS, Veritas, Lloyd namely):

  • 2 Hz to 13.2 Hz with an amplitude of +/- 1 mm (+/- 0.04 in)

  • 13.2 Hz to 100 Hz at a constant acceleration of 0.7 g

Electromagnetic Disturbances

ComPact NSX circuit breakers are immune to electromagnetic disturbance.

They comply with the requirements of the electromagnetic compatibility (EMC) standard:

Standard

Title

IEC/EN 60947-2 appendixes F and J

Overcurrent protection tests

IEC/EN 60947-2 appendixes B and J

Specific tests for earth-leakage protection

Check for compliance with EMC standards by testing for immunity to:

  • Overvoltages produced by the operation of electromagnetic switchgear.

  • Overvoltages produced by atmospheric disturbance that pass through the electrical network (for example, lightning).

  • The use of apparatus emitting radio waves (such as radio transmitters, walkie-talkies, or radar).

  • Electrostatic discharges produced by the operators themselves.

Conformity with EMC standards as described above helps to ensure that:

  • The circuit breaker operates correctly in a disturbed environment:

    • Without nuisance tripping.

    • In accordance with the trip time.

  • There is no disturbance to any type of industrial or commercial environment.

Altitude

ComPact NSX circuit breakers are designed to operate within specification at altitudes of up to 2,000 m (6,600 ft).

Above 2,000 m (6,600 ft) modifying the characteristics of the surrounding air (dielectric strength, cooling capacity) causes derating as follows:

Altitude (m/ft)

< 2,000 m

(6,600 ft)

3,000 m

(9,800 ft)

4,000 m

(13,000 ft)

5,000 m

(16,500 ft)

Maximum operating voltage (V)

690

590

520

460

Maximum operating voltage (V) for NSX400K

1000

886

790

696

Rated thermal current (A) at 40 °C (104 °F)

In

0.96 x In

0.93 x In

0.9 x In

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.