DOCA0140EN-03

TM-D Thermal-Magnetic Trip Unit for 3P and 4P Circuit Breakers from 80 A to 250 A

Introduction

The TM-D thermal-magnetic trip unit is designed to protect conductors in commercial and industrial electrical distribution.

The trip unit exists in two configurations:

  • 3P, 3D

  • 4P, 3D

Description

The adjustment dials are on the front of the trip unit:

A Setting range for the TM-D thermal-magnetic trip unit

B Adjustment dial for the thermal protection pickup Ir

C Adjustment dial for the magnetic protection pickup Ii (for TM-D 200/250 only)

Setting the Thermal Protection

The thermal protection pickup Ir is set by a 4-setting dial.

Turning the thermal protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pickup Ir (in amperes) for thermal protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ir.

Trip unit rating In (A)

16

25

32

40

50

63

80

100

125

160

200

250

Pickup Ir (A)

11

18

22

28

35

44

56

70

88

112

140

175

13

20

26

32

40

50

64

80

100

128

160

200

14

23

29

36

45

57

72

90

113

144

180

225

16

25

32

40

50

63

80

100

125

160

200

250

Setting the Magnetic Protection on Trip Units with In from 80 A to 160 A

For trip units rated below 200 A, the magnetic protection pickup cannot be adjusted and equals the value shown below:

Trip unit rating In (A)

16

25

32

40

50

63

80

100

125

160

Pickup Ii (A) +/- 20%

190

300

400

500

500

500

640

800

1250

1250

Setting the Magnetic Protection on Trip Units with In from 200 A to 250 A

For trip units rated between 200 A and 250 A, the magnetic protection pickup Ii is set using a 6-setting dial.

Turning the magnetic protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pickup Ii (in amperes) for magnetic protection (values indicated on the dial), relative to the position of the Ii dial:

Trip unit rating In (A)

200

250

Pickup Ii (A) +/- 20%

1000

1250

1200

1500

1400

1750

1600

2000

1800

2250

2000

2500

Example of Application

Protection of a feed with the following characteristics:

  • Power supplied by a 1,250 kVA transformer - 400 V, 4%

  • Protection of a distribution box located 15 m away, the loads on which are mainly for lighting (incandescent bulbs), heating, and small machines

The value of the calculated rated current (load consumption) is In = 175 A.

The following illustration shows the installation diagram:

Calculations performed on the installation in accordance with the regulations can be used to determine the characteristics of the appropriate ComPact NSX circuit breaker to install (calculations performed using the Ecostruxure Power Design – Ecodial software).

The following table presents the circuit breaker selection:

Installation

Chosen ComPact NSX

Comments

In = 175 A

ComPact NSX250

Determination of case size

Distributed neutral

4P, 3D

Full neutral and linear loads

Isc = 28.5 kA

F

Icu performance can be read from rating plate

Ikmin = 14.0 kA

The following table shows the trip unit protection settings:

Installation

Chosen trip unit

Comments

In = 175 A

TM-D 200, Ir set to 180 A

Optimizing the choice

TM-D 250, Ir set to 175 A

Necessary if extensions envisaged

Ikmin = 14.0 kA

Ii = 2,000 A or 2,500 A

Natural adjustment to the Ii protection for distribution, compatible with:

  • Inrush currents (no trip)

  • Short-circuit protection (trip)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.