DOCA0140EN-03

Insulated NSX Cord

Introduction

For system voltage greater than 480 Vac, an insulated variant of the NSX cord needs to be used, terminated by an electronic module with a female RJ45 connector. A ULP cord must be used to connect the insulated NSX cord electronic module to a ULP module.

The reference for the insulated NSX cord is LV434204.

The insulated NSX cord electronic module must be supplied with 24 Vdc in order to guarantee isolation of the ULP system.

NOTE: The insulated NSX cord cannot be installed in a ComPact NSX400K circuit breaker.

For more information about installation, consult the instruction sheet on the Schneider Electric website: GHD16313AA ComPact NSX100–630 – Insulated NSX Cord.

Electronic Module Characteristics

The following table summarizes the electronic module characteristics:

Characteristic

Value

Dimensions

27 x 27 x 27 mm

Mounting

On DIN rail

Degree of protection of the installed module

  • On the front panel (wall-mounted enclosure): IP40

  • On the connections (behind the enclosure door): IP20

Operating temperature

-25 to +70 °C

Power supply voltage

24 Vdc -20%/+10% (19.2–26.4 Vdc)

Consumption

  • Typical: 20 mA/24 Vdc at 20 °C

  • Maximum: 30 mA/19.2 Vdc at 60 °C

Insulated NSX Cord Connection

The NSX cord connects to a ULP module:

  • IFM or IFE communication interface

  • FDM121 display

  • IO module

The figure below illustrates the connections from the insulated NSX cord to the Modbus-SL interface for one circuit breaker:

A IFM Modbus-SL interface for one circuit breaker

B RJ45 male/male ULP cable

C Insulated ULP module for system voltage greater than 480 Vac

D Insulated ULP cord for system voltage greater than 480 Vac

E Connector for ComPact NSX circuit breaker internal connection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.