DOCA0140EN-03

Applications

The Two Main Types of Application Requiring Protection

ComPact NSX circuit breaker trip units offer protection for all applications due to the great flexibility of their settings.

Two types of application are taken into consideration:

  • Electrical distribution protection

  • Specific protection for receivers (for example, motors, transformers) or generators

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.