DOCA0140EN-03

USB Maintenance Interface Connected to a PC

Description

Use the USB maintenance interface connected to a PC running EcoStruxure Power Commission software to carry out the complete range of checks, tests and adjustments on the MicroLogic trip unit.

There are two possible ways to connect the PC to the USB maintenance interface:

  • Using the USB port

  • Using the Bluetooth/Modbus option

NOTE: The USB maintenance interface cannot be used with the MicroLogic 2.3 trip unit installed in a ComPact NSX400K circuit breaker.

Connection Using USB Port

A PC running EcoStruxure Power Commission software

B USB maintenance interface

C Trip unit test port

D MicroLogic cord for connecting the USB maintenance interface to the test port on the trip unit

E USB standard connection cable from the USB maintenance interface to the PC

NOTE: If the USB port does not supply enough power to energize the MicroLogic trip unit and the USB maintenance interface, the three test LEDs on the USB maintenance interface start to blink. In such cases, provide energy to the USB maintenance interface from the power supply module supplied with the USB maintenance interface kit.

Connection Using Bluetooth/Modbus Option

A PC running EcoStruxure Power Commission software

B USB maintenance interface

C Trip unit test port

D MicroLogic cord for connecting the USB maintenance interface to the test port on the trip unit

E PS/2/RJ45 cord for Bluetooth/Modbus option, on the USB maintenance interface

NOTE: Use the power supply unit supplied with the kit.
NOTE: Connect the Bluetooth/Modbus option firmly to the PS/2 connector on the USB maintenance interface. Do not force the mechanical cap in order to use the RJ45 connection on the USB maintenance interface. It is used for the ULP connection method only.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.