DOCA0140EN-03

ComPact NSX100-630 - Reflex Tripping

Presentation

ComPact NSX circuit breakers incorporate the exclusive reflex-tripping system.

This system breaks very high fault currents.

The circuit breaker is mechanically tripped via a “piston” actuated directly by the short-circuit.

For high short-circuits, this system provides a faster break, thereby ensuring selectivity.

Reflex-tripping curves are exclusively a function of the circuit breaker rating.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.