Opening, Closing, and Resetting a Circuit Breaker With Motor Mechanism
Introduction
The motor mechanism can open and close a circuit breaker remotely with electrical commands. There are many applications:
-
Automation of electrical distribution to optimize operating costs
-
Normal/standby source changeover: changes over to a replacement source to improve continuity of service
-
Load shedding/reconnection to optimize tariff-based contracts
![]() |
---|
HAZARD OF REPEATED CLOSING ON ELECTRICAL FAULT
Do not modify the wiring diagrams for the motor mechanism.
Failure to follow these instructions can result in injury or equipment damage.
|
Wire the motor mechanism in strict accordance with the motor mechanism wiring diagram in the appendix.
In automatic operating mode, wiring the SDE contact helps to prevent the circuit breaker from resetting automatically on an electrical fault. For more information about the SDE contact, refer to the indication contacts.
Manual Operation: Opening, Closing, and Resetting Locally
Move the selector to the Manu position.
Manual Operation Description
Check that the spring-charged indicator is on A). If not, reset the circuit breaker.
(Automatic Operation: Opening, Closing, and Resetting Remotely
Automatic Operation Description
Step |
Action |
Comment |
---|---|---|
1 |
Close the circuit breaker by sending a close ( ) command. |
When the circuit breaker is closed:
|
2 |
Open the circuit breaker by sending an open ( ) command. |
When the circuit breaker is open:
|
3 |
Recharge the stored energy control by using one of the three reset modes, depending on the wiring diagram:
|
The circuit breaker is ready to be closed:
|
Resetting After a Trip on Electrical Fault
Resetting after a trip on electrical fault can only be done locally. When operating in automatic mode, return to manual operation to reset the circuit breaker.
![]() |
---|
HAZARD OF CLOSING ON ELECTRICAL FAULT
Do not close the circuit breaker again without first inspecting
and, if necessary, repairing the downstream electrical equipment.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The fact that a protection has tripped the circuit breaker does not remedy the cause of the fault detected on the downstream electrical equipment.
To reset after a fault trip:
Step |
Action |
---|---|
1 |
Isolate the feed before inspecting the downstream electrical equipment. |
2 |
With selector on Manu, operate the charging handle 8 times to reset the circuit breaker in ready-to-close position. Result: The spring-charged indicator changes to charged (B) and the internal mechanism goes from the Trip position to the O (OFF) position (A). |
3 |
Lock the circuit breaker. |
4 |
Look for the cause of the detected fault. |
5 |
Inspect and, if necessary, repair the downstream equipment. |
6 |
Inspect the equipment in the event of a short-circuit trip. |
7 |
Reset and close the circuit breaker. |