Withdrawable Circuit Breaker
Introduction
In addition to the advantages provided by a plug-in base, installation of the circuit breaker on a chassis facilitates handling. Withdrawable chassis circuit breakers offer three positions, with transfer from one to the other after mechanical unlocking:
-
Connected: the power circuits are connected.
-
Disconnected: the power circuits are disconnected, the circuit breaker can be operated to check auxiliary operation.
-
Removed: the circuit breaker is free and can be removed from the chassis.
The following types of circuit breaker can be installed in a chassis:
-
3P and 4P circuit breakers
-
Circuit breakers with toggle handle, direct rotary handle, or extended rotary handle
-
Motor-operated circuit breakers
-
Circuit breakers with VigiPacT Add-on
The withdrawable circuit breaker is made up of:
-
The fixed circuit breaker
-
A plug-in kit
-
Two chassis side plates for the plug-in base
-
Two chassis side plates for the circuit breaker
For more information about withdrawable circuit breaker installation, consult the instruction sheets on the Schneider Electric website:
-
GHD16277AA, Chassis side plates for ComPact NSX100-250
-
GHD16317AA, Chassis side plates for ComPact NSX400-630
Plug-in Kit and Chassis Installation Demonstration Video
To access a demonstration video about the installation of a plug-in kit and chassis for withdrawable ComPact NSX100-250 circuit breakers, click the following link: https://youtu.be/XaXO6QgeWvM, copy and paste the link to your Web browser, or scan the QR code.
Disconnecting the Circuit Breaker
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow this procedure to disconnect the circuit breaker:
Step |
Action |
|
---|---|---|
1 |
Switch the circuit breaker to the O (OFF) position. |
|
2 |
Move both locking levers down as far as they can go. |
|
3 |
Push down both operating handles at the same time until you hear a double-click from the locking levers (as the locking levers return to their original position). The circuit breaker is disconnected. |
-
The auxiliary circuits can be:
-
Automatically disconnected because of the connectors located on the chassis and at the rear of the circuit breaker.
-
Left connected for a circuit breaker with a manual auxiliary connector.
-
-
Open the circuit breaker before disconnecting it. If the circuit breaker is in the closed I (ON) position when disconnecting, a safety mechanism ensures that the poles open automatically by tripping the circuit breaker before the pins disconnect.
Removing the Circuit Breaker
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow this procedure to remove the circuit breaker:
Connecting the Circuit Breaker
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow this procedure to connect the circuit breaker:
Step |
Action |
|
---|---|---|
1 |
Switch the circuit breaker to the open O (OFF) position. Move both operating handles down to the low position on the chassis. Push in the circuit breaker until the locking levers clicks. |
|
2 |
Move both locking levers forward. |
|
3 |
Raise both locking levers at the same time. |
Withdrawable Circuit Breaker Protection Against Direct Contact With Power Circuits
The following table shows withdrawable circuit breaker configurations with the corresponding protection indices (IP):
Configuration |
Protection index |
Description |
---|---|---|
IP20 |
Built-in chassis:
|
|
IP40 |
Built-in chassis and circuit breaker with terminal shields. |
|
IP40 |
Chassis with adapter, terminal shields and blanking plate without circuit breaker:
|
|
IP40 |
Chassis with adapter and terminal shields, and circuit breaker with terminal shields. |
Auxiliary Circuit Test with Circuit Breaker Disconnected (Optional)
The auxiliary circuit test function is possible with circuit breakers which have manual auxiliary connectors.
In the disconnected position, operate the circuit breaker (by the actuator or push-to-trip button) to check whether the auxiliary circuits are working correctly.
Disconnect the manual auxiliary connector (if the circuit breaker has one) before removing the circuit breaker.
Carriage Switches (Optional)
Two changeover contacts can be installed on the chassis:

A Connected-position carriage switch (CE)
B Disconnected-position carriage switch (CD)
For more information about contact operation, refer to control auxiliaries.
Carriage switches, in conjunction with the IO module, provide the chassis management function, which is used to:
-
Record and check the position of the moving part of the withdrawable circuit breaker in the chassis
-
Provide information about preventive maintenance actions
-
Notify the remote controller about the position of the withdrawable circuit breaker.
For more information about the chassis management function, refer to DOCA0055EN, Enerlin'X IO - Input/Output Application Module for One IEC Circuit Breaker - User Guide,
Locking the Chassis
The operating handle can be locked with up to four padlocks (not supplied) or keylock.
Illustration |
Description |
---|---|
Lock the circuit breaker in disconnected position using up to four padlocks (not supplied) with a shackle diameter of 5–8 mm (0.2–0.3 in) to prevent connection. |
|
Lock the circuit breaker using a keylock (optional) in the connected position when the locking kit accessory is installed. |
|
Lock the circuit breaker using a keylock (optional) in the disconnected position when the locking kit accessory is installed. |
For more information about the accessory offer, refer to LVPED217032EN, ComPact NSX & NSXm Catalogue.