Accessories
Accessories for ComPact NSX Circuit Breakers
A comprehensive accessory offer is available for ComPact NSX circuit breakers. Accessories can be installed on site to improve safety and ease of operation.
For more information about the accessory offer, refer to LVPED217032EN,ComPact NSX & NSXm Catalogue.
Long Terminal Shields with Precut Grids
Terminal shields with precut grids simplify the onsite connection of circuit breakers regardless of the number of conductors to be connected. The procedure for installing precut grids is described in the following instruction sheets on the Schneider Electric website:
-
GHD16242AA, ComPact NSX100–250 circuit breaker and switch-disconnector
-
GHD16243AA, ComPact NSX400–630 circuit breaker and switch-disconnector
Short Terminal Shields
The procedure for installing short terminal shields is described in the following instruction sheets on the Schneider Electric website:
-
GHD16242AA, ComPact NSX100–250 circuit breaker and switch-disconnector
-
GHD16243AA, ComPact NSX400–630 circuit breaker and switch-disconnector