DOCA0096EN-02

Electrical Auxiliary Devices

Summary of Electrical Auxiliary Devices

The following table shows electrical auxiliary devices that can be added to circuit breakers. Electrical auxiliary devices can be installed on site. For more information, see LVPED217032EN, ComPact NSX & NSXm Catalogue.

Electrical auxiliary device

Use

3P/4P circuit breaker

3P/4P ELCB

OF indication auxiliary (wired or wireless)

View the on/off status of the circuit breaker remotely.

SD indication auxiliary (wired or wireless)

View the trip status of the circuit breaker remotely.

MX shunt trip

Send an electrical trip command remotely.

MN undervoltage release

Trip the circuit breaker when the control voltage drops below a tripping threshold.

MN undervoltage release with time-delay unit

Intended to avoid nuisance tripping in systems with frequent voltage dips lasting from 200 ms to 3 s.

SDx module

Provide alarm and fault differentiation for the ComPact NSXm earth-leakage circuit breaker.

Slots for Electrical Auxiliary Devices for Circuit Breaker

The following figures show the available slots for electrical auxiliary devices mounted in the circuit breaker case. One auxiliary can be installed in each slot. For more information, see LVPED217032EN, ComPact NSX & NSXm Catalogue.

3P circuit breaker

4P circuit breaker

A MN undervoltage release or MX shunt trip

B OF indication auxiliary (wired or wireless)

C SD indication auxiliary (wired or wireless)

Slots for Electrical Auxiliary Devices for Earth-Leakage Circuit Breaker

The following figures show the available slots for electrical auxiliary devices mounted in the case of the earth-leakage circuit breaker (ELCB). One auxiliary can be installed in each slot.

3P ELCB

4P ELCB

A MN undervoltage release or MX shunt trip

B OF indication auxiliary (wired or wireless)

C SD indication auxiliary (wired or wireless)

The following figures show the available slots for electrical auxiliary devices mounted outside the earth-leakage circuit breaker (ELCB). Two SDx modules can be installed.

3P ELCB

4P ELCB

A SDx module (1 or 2 maximum)

For more information, see LVPED217032EN, ComPact NSX & NSXm Catalogue.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.