Opening, Closing, Resetting, and Testing the Circuit Breaker
Opening and Closing with the Side Rotary Handle
Resetting with a Side Rotary Handle After a Trip
Testing the Trip Mechanism
CAUTION |
|---|
|
HAZARD OF NUISANCE TRIPPING
Circuit breaker tests must only be done by qualified electrical
personnel.
Failure to follow these instructions can result in injury or equipment damage.
|
When testing the trip mechanism take precautions against:
-
Disrupting operations
-
Activating inappropriate alarms
-
Triggering unwanted actions
For example, tripping the circuit breaker with the push-to-trip button can lead to inappropriate fault indications or corrective actions (such as switching to an alternate power source).
There is no push-to-trip button on the door of a circuit breaker with a side rotary handle. To check the trip mechanism, the door must first be opened.
Follow these steps to test the trip mechanism.



CAUTION