Clearance Requirements for ComPact NSXm Circuit Breakers
Introduction
When installing ComPact NSXm circuit breakers in equipment, minimum distances (safety clearance) must be maintained between the device and panels, bars, or any metal installed nearby.
Minimum distances depend on the ultimate breaking capacity, and are defined by tests carried out in accordance with the IEC/EN 60947-2 standard.
If IEC/EN installation conformity is not checked by type tests, you must also:
-
Use insulated bars for circuit breaker connections.
-
Block off the busbars by using rear insulation screens.
Equipment Installation Requirements
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Follow these guidelines when installing circuit breakers in equipment:
-
Respect minimum distances.
-
Perform dielectric strength tests, thermal calculations, and temperature rise tests as required by the configuration of the installation.
-
Respect the limits defined in the derating tables, depending on the ambient temperature (ratings are based on IEC/EN 60947-2 standard).
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Install circuit breaker so minimum clearance distance
to grounded metal is maintained.
Failure to follow these instructions will result in death or serious injury.
|
Minimum Distances for Side-by-Side Installation
Minimum Clearance Without Insulation Accessories
The minimum clearance distances required around circuit breakers without insulation accessories are shown below.
Minimum Clearance with Interphase Barriers
The minimum clearance distances required around circuit breakers equipped with interphase barriers are shown below.
Minimum Clearance with Long Terminal Shields
The minimum clearance distances required around circuit breakers equipped with long terminal shields are shown below.
Minimum Clearance to Bare Busbars
The minimum clearance distances required around circuit breakers that use busbars are shown below.
Minimum Clearance Between Backplate and Uninsulated Power Connections
For all types of ComPact NSXm circuit breakers that use uninsulated power connections (for example, busbars, spreaders, or uninsulated crimped lugs), the minimum clearance distance with the enclosure backplate is shown below.
ew graphics
A rear insulation screen or long terminal shield is required if the distance C is less than 8 mm (0.32 in).
DANGER